VBUS.ACNOMINAL
Description
This command configures the operating voltage for a level other than the default of the drive.
-
-
The drive can be de-rated but do not operate it higher than the original voltage.
When changed, VBUS.ACNOMINAL modifies the inrush voltage settings and the regen voltage configurations. It is important that VBUS.ACNOMINAL be set as accurately as possible to minimize voltage faults.
Examples
Code
If an HV drive (480V) was needed for bench testing at 120V, do the following:
VBUS.ACNOMINAL 120
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
VAC |
|
Range |
0 to Drive rated voltage |
|
Default Value |
Drive rated voltage |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.